Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide9

The SPORT is the high speed Blackfin synchronous serial port. It features fully independent transmit and receive channels, and as we see on the right hand side of the figure, each side of the interface, the transmit and the receive side, consist of four pins. So there’s the primary data, the secondary data, the clock and the frame sync. And we have four for transmit, four for receive.

PTM Veröffentlicht am: