Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide29

Here is a representation of a video frame both for NTSC and PAL under the 656 recommendation. This shows that the horizontal blanking region is demarcated by the H bit, so EAV or End of Active Video is when H equals 1. The transition to H equals 0 is the SAV, the Start of Active Video. Likewise when V changes from 1 to 0 it denotes a new region, blanking versus active video. Then the field, Field 1 and Field 2 are also denoted by the change between 0 and 1 on the F line. These control codes are sent in the data stream, along with the data. If you were to take a snap shot of the data stream you would see a few leading bytes, (we’re looking at an 8-bit case of 8-bit video components). “FF 00 00” -- that’s the preamble associated with a control code. It lets the end device know that a control code is coming.

PTM Veröffentlicht am: