Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide34

You can also optionally ignore the second field of an interlaced stream. This can be useful in some applications where data quality or video quality is not as important as the compression that you can achieve by doing this, by using only Field 1 of every frame. You can also skip even or odd data elements, so you can read in only the luma or only the chroma of a 4:2:2 input stream. The whole PPI peripheral works hand in hand with the concept of the 2 dimensional DMA engine that Blackfin has. This allows to specify an arbitrary region of memory and send it out to the PPI without having to worry about parts that you do not want to send out. For example, you can specify an arbitrary rectangular region of an image and send it out the PPI.

PTM Veröffentlicht am: