Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide43

Instead, at the panel side, you can tie the least bit of red to the most significant bit of red and do the same for blue, tie the least significant bit to the most significant bit. When you do this, it will ensure that you’ll get a full dynamic range from the very lowest to very highest value on each of those channels. Whereas with green, you are connecting 6-bits. All 6-bits get passed through on the green channel because green is considered the most visually important channel of the three.

PTM Veröffentlicht am: