Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide31

The PPI on Blackfin is the video port that handles this information. PPI stands for the parallel peripheral interface. It is a video interface, however it generally supports high speed parallel converter interfaces. In the generic sense it is a high speed parallel port and has some nice video friendly features as well. It is a pretty straightforward interface, consisting of 16 data lines, PPI15 through 0 in this picture. There are up to three frame syncs, the PPI_FS1, the_FS2, and the _FS3 and then the clock, PPI_CLK. This clock is always sourced externally to the PPI, but the frame syncs and the data, depending on the mode you’re operating in, can be either inputs or outputs. On some of the subsequent slides, in the 656 modes of operation these frame sync lines are not required because everything is embedded in the data stream.

PTM Veröffentlicht am: