Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide40

The PWM timer block that you see up on top is an optional connection. These TFT-LCDs for reason of cost or footprint will not integrate a timing controller, which means that you buy the TFT module as well as a separate timing ASIC to go along with it, which is added cost into the system. In these cases where the TFT module does not support the timing controller directly, the Blackfin can supply these signals through some extra timers. It would be on the order of what you see here, a signal to start sampling, a signal to denote the scan direction and maybe a clock for gate drivers.

PTM Veröffentlicht am: