Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide23

The most popular color space supported and the one that BT.601 prefers is the YCbCr color space. Where Y equals the luma component and the Cr or Cb equals the chroma component. These signals are generated via RGB in a mathematical relationship and they are highly uncorrelated, which means that they provide much better compression characteristics than RGB information does. That’s one of the key reasons that this color space is so popular, and is recommended by BT.601.

PTM Veröffentlicht am: