Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide34

Let’s look at connecting up to some video sources. There is not too much difference from what we’ve seen before in the general sense, we have the control channel here where we are looking at a CMOS image sensor. The control channel in this diagram is through the two wire interface that connects to the sensor’s I²C bus. That is used for configuration of the device where the actual data flows straight into the 8-bit PPI in this case. There’s no reason that this couldn’t be a 10-bit, 12-bit, or even 16-bit application, depending on the resolution of the sensor, of the imager that you’re connecting to. But this diagram shows an 8-bit connection. The imager in this case usually will provide the pixel clock as well as some kind of framing. The horizontal sync will demarcate the valid line region and the Vsync will be a “frame valid” type of signal. Of course many sensors also support the BT.656 standard in which case these synchronization signals are not needed.

PTM Veröffentlicht am: