Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide41

Here are some tips and tricks to help connect up to video sources and displays. First, use BT.656 whenever possible because it eliminates a lot of timing incongruities and inconsistencies that can crop up in an application. So when you have the choice, go for 656. Also pay close attention to the default converter settings for whatever A to D or D to A you’re using because often times you’ll find that you might be operating in a mode that you didn’t expect. A lot of times you’ll be able to use these converters directly without programming through an I²C or SPI interface, but sometimes you’ll also want to verify through the feedback channel of I²C that you do have the device configured to the appropriate settings.

PTM Veröffentlicht am: