Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide6

There are two main types of serial interfaces on Blackfin that are relevant in the audio world, one is a low bit rate interface that is used for control and configuration of audio devices, and another is a higher bit rate peripheral that’s used for the actual data interchange. On the control and configuration front there are two peripherals in high usage, one is the two wire interface, the TWI, and the other is the serial peripheral interface, or SPI. In general the forward channel of these peripherals is used to configure or control an audio converter, and the reverse channel relays feedback or status information from the converter. The SPORT (what we call it on Blackfin) is a synchronous serial port and used as a data channel for audio data. It can operate at high bit rates and its full duplex supports both transmit and receive applications, and can do so simultaneously. In some codec, like the popular PC AC97, the SPORT also serves as the control channel for the codec.

PTM Veröffentlicht am: