Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide18

Some additional collateral for audio development that you definitely would want to look into from a software side would be the Visual DSP++ tool suite which includes many peripheral drivers including the two wire interface, SPI, SPORT and others, that allow via a standard API, to configure and control those interfaces. There are complete audio device drivers included under VisualDSP, and provides a standard API for audio converters. Many devices are supported, and more are being added continually. On the EZ-KIT, the Blackfin EZ-KITs and EZ-Extender cards that plug on top of the EZ-KIT, there are many code examples that come with those platforms, and they show how to integrate these peripheral and these converter device drivers. They also provide really good examples of data flows and how to configure your system when you have a lot going on and provide a very useful framework.

PTM Veröffentlicht am: