Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide21

An analog camera source first has to pass through a video decoder, and it’s just an A to D converter, which digitizes the stream for input into the Blackfin. Like a CCD sensor, it will also pass through an analog to digital converter called an AFE, or an analog front end. On the bottom, in the video display realm the Blackfin can natively send a digital stream out to something like a TFT-LCD display which accepts digital input. If it’s going to something like a CRT or some kind of TV or analog display, then it must first pass through a hardware encoder, a video encoder, which is a D to A converter.

PTM Veröffentlicht am: