Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide22

The ITU recommendation for digital television is BT.601. That was the recommendation that specified from a broadcast perspective, how to encode digital television signals. It supports a couple of color spaces, the most obvious one is RGB, red, green and blue, which is very intuitive, but there’s a lot of correlation between the channels and it’s not really the best one to use for compression. And the format -- when you say RGB888 format, this implies 8-bit each for the red, green, and the blue component. If we say RGB666 this means that there are 6-bits each of those per pixel and 565 means there are 5 for red and blue, but there are 6 for green.  We’ll talk more about that in our LCD discussion.

PTM Veröffentlicht am: