Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide42

It is also very important to make sure in whatever you’re doing the clock source is as clean as possible. These clock rates are pretty high, they’re in the several MHz to tens of MHz depending on your application. A clean clock can make a huge difference in the success and the stability of an application from a system viewpoint. Finally, when you hook the Blackfin to an LCD panel as a 666 LCD, 6-bits of R, G and B for a total of 18-bits, the Blackfin connects as a RGB565 device. When you do this, do not ground the least significant bit of the red and the blue channel. This is a common practice that is not ideal in terms of the dynamic range that you’re representing.

PTM Veröffentlicht am: