Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide7

The Blackfin peripheral is compatible with the Motorola SPI standard. It is a full duplex serial interface and operates up to 33Mbits per second, which is usually well beyond what most converters need for any type of control. It supports both masterslave and multi-master environments, and really only consists of a three pin data communication interface. The MOSI, is the output from a master that is an input to the slave device. The MISO, is the input to a master from a slave, and then there’s the serial clock, the SCK line. In order to enable the master and slave side of things, the SPI chip select input is used when the Blackfin is a slave to some other SPI device. The SPI device will select the Blackfin through that line. When the Blackfin is the master, it will use one of it’s many SPISEL lines, or one of its slave select lines, which allows it to select any number of other devices. Usually a processor will have on order six or seven of these slave select lines.

PTM Veröffentlicht am: