Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Interfacing-AV-Slide30

The “AB” in this picture is really just the pertinent control code that tells if H is changing, if V or F is changing and there are some checksum bits in there for error correction as well. If we’re at the start of a line, you’ll see a long sequence of horizontal blanking, which is denoted by the “80 10 80 10” sequence. Then there’s another preamble code that tells the system that H=0, the SAV (the start of active video) is coming. Then there will be the whole video line, the 720 active pixels which equates to 1440 bytes. And then we’re off to the start of the next line with a new end of active video sequence.

PTM Veröffentlicht am: