Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 36

Until recently, the L6470 was the monolithic solution featuring the voltage mode, the L6472 was the monolithic solution for the current mode. However, a monolithic solution is limited to 45 V and 3 A. If the application requires higher power, the L6480 will drive the motor in the voltage mode and the L6482 will do so in the current mode. The designer simply needs to choose the appropriate part based on the system requirements.

PTM Veröffentlicht am: