Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 27

The voltage mode allows the design of a stall detection. As explained previously, the Back EMF must be compensated and the faster the motor spins the higher the applied voltage is in order to get a stable current. If the motor stalls, the Back EMF is not present anymore but the powerSTEP01 continues to apply the same voltage. This triggers an increase in the current that is detected. The stall detection threshold is programmable. Based on the characteristics of the motor and the speed of the motor, a stall detection threshold can be calculated. If the current is above this threshold, that means the motor is stalled.

PTM Veröffentlicht am: