Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 10

A decay is accomplished by applying a given voltage to the coil in order to decrease the current in the coil. Depending on the voltage that is applied, there are two types of decay. Using the equation U = l x dI/dt, it is shown that the higher the voltage is, the faster the current will increase or decrease. When a system recirculates the current in a high or low side of an H-bridge, a small voltage is applied to the coil, which is a slow decay. When the inverse of the DC bus is applied to the coil, the voltage is high, called fast decay.

PTM Veröffentlicht am: