Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 29

The Digital Motion Engine is a group of high level commands that decrease dramatically the workload on the microcontroller. With the motion engine, the microcontroller sends the commands through an SPI bus. In order to work correctly, some registers must be programmed, such as the minimum speed, the maximum speed, as well as the acceleration and deceleration when the motor spins.

PTM Veröffentlicht am: