Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 25

The principle of the voltage mode is to apply a calculated voltage to reach a target current. The applied voltage is a percentage of the DC bus; therefore three parameters must be taken into account. The Back EMF as explained previously. If the DC bus is changing, the percentage must be changed. If the DC bus lowers, the percentage must be increased. This is done thanks to an embedded ADC. As the voltage across the resistance of the motor changes the voltage across the coil of the motor, if the resistance of the motor changes through the temperature, this must also be compensated. The powerSTEP01 has a register to compensate the change of resistance.

PTM Veröffentlicht am: