Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 13

The powerSTEP01 can drive at up to 85 V, high for a stepper motor. The RdsON of each MOSFET of the bridge is 16 mΩ, compared with 300 mΩ for a typical monolithic solution. dSPIN introduced the voltage mode to the market; the traditional method is the current mode. Two powerSTEP01 part numbers exist, the L6470 for voltage mode and L6472 for current mode. The following slides will highlight both modes as this is a key feature that makes the powerSTEP01 unique. Due to the low RdsON, The powerSTEP01 can drive up to 10 A, unlike a monolithic solution that can drive up to 3 A at best. The current of the gate drivers can be programmed to optimize EMI and switching losses. In the voltage mode, 128 microsteps is available for smooth operation.

PTM Veröffentlicht am: