Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 23

This slide presents the difference between the two modes. The traditional mode is the current mode. In voltage mode, the voltage is applied though a fixed frequency PWM. When switched from one current level to the next current level, can take several cycles which provides smooth operation with less ripples and no audio noise as it is a fix frequency PWM. Thanks to the small ripples, 128 microsteps are possible. The current mode is more noisy and the frequency of the PWM can change and appear in the audible range. The current mode behaves better and keeps a higher torque at high speed. In low speed, the voltage mode is smoother and allows a better torque regulation at very low speed.

PTM Veröffentlicht am: