Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 15

The block diagram of the L6470, called dSpin for digital spin, is shown on this slide. This block diagram is similar to all of the family, including the powerSTEP01, it integrates a dual H-bridge, dual thermal protection (one warning and one shut down), and over current protection. Major innovations particular to the dSpin are a voltage control mode that allows a true 128 µsteps, the voltage mode does not monitor the current in the bridge; hence, it is a not dissipative current sensing design, and the capability to program the position and the speed profile of the motors.

PTM Veröffentlicht am: