Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 21

An issue with current control is that when the target current is reached, the decay is applied. This means the average current is lower than target current and hence, the position is not exactly the expected position. Predictive current control solves this problem. Based on the previous two cycles and how long it takes to reach the target current, the bridge stays ON for an extra time before the decay is applied. This allows the average current to be truly the target current.

PTM Veröffentlicht am: