Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 14

The challenge was previously presented to control the current in a stepper motor. Thanks to dSPIN, easySPIN, and powerSTEP01, this is no longer such a challenge; it is in fact easy. When an engineer designs a stepper motor driver, the various challenges are the timing of the decays, if slow or fast decay must be applied, and the parameters that depend on the Back EMF, related to speed and torque. This has an impact on the frequency of the PWM and if not properly performed can create a power dissipation issue. All these interleaved parameters can be very challenging for creation of the code for the microcontroller. The new easySPIN and dSPIN greatly simplify the design process.

PTM Veröffentlicht am: