Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 24

As shown previously, in voltage mode, the Back EMF must be known. Hence, a Back EMF compensation must be performed. If not performed, the current decreases as the motor spins faster. When the powerSTEP01 drives the motor, by using the motion engine, the device knows the speed of the motor, and the Back EMF that is proportional to the speed of the motor. In real time, it can calculate what voltage to apply in order to get a stable current. The faster the motor spins, the higher the applied voltage is.

PTM Veröffentlicht am: