Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 30

Many commands are available. For example, there is the Move command. If the application requires the motor to move 1000 steps in a given direction, a simple 4 byte Move command is sent by the microcontroller and all the motion will be calculated and driven by the powerSTEP01 based on the acceleration, deceleration, maximum speed and minimum speed. If the application requires the motor to go to an absolute given position, the GoTo command performs the task. The GoTo chooses the shortest path and the GoTo_DIR forces the direction of the motor.

PTM Veröffentlicht am: