Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 22

In the previous slides, the current mode was presented. In this mode, the current is directly measured and actions are performed based on this measurement. The second method is the voltage mode, in which the current is not measured. Shown on the left side of this slide is the schematic of a stepper motor; VPH is the voltage applied to the motor, Rm the resistance of the motor, Lm the inductance of the motor, and the Back EMF of the motor. On the right is the vector representation of the system. The principle of the voltage mode is, knowing the fixed values of BEMF, resistance, and inductance of the motor, and having a target current, the voltage to apply is calculated to reach the target current.

PTM Veröffentlicht am: