Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 6
Here is an IrDA Standard system. Starting on the right we have the Primary Device, in this case a PDA. Left of the PDA we have the embedded system, which is the IrDA Standard Secondary Device. This Embedded System can be broken into three parts: The IR side with Optical Transceiver, The Protocol Handler, and The Host Controller side, which includes Host UART.
PTM Veröffentlicht am: