Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 16
Discovery is the state where the Primary Device and the Secondary Device determine each other’s capabilities. First the Primary Device transmits an SNRM command with parameters and connection addresses. The Secondary Device will then issue a UA response with parameters using the specified connection address. The Primary Device then Opens a channel for IAS Queries, which the Secondary Device will confirm.
PTM Veröffentlicht am: