Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 10
Then we add the Application layer. At the Application layer is where there are different Application Protocols. You can think of these application protocols as languages. If two devices try to communicate, and they are not using the same protocol or  language, they will not be successful. When many people think infrared, they think “Beaming”. That is when they select an Object to “beam” to another device. This technique actually uses IrObex, which stands for IR Object Exchange. In this case the characteristics of the “Object” (file, program, photo) are know before the object is transferred.
PTM Veröffentlicht am: