Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 18
On a PC this will only occur after a PC program has “attached” to the IR port - such as HyperTerminal. On a PDA this occurs when the 1st byte (packet) of data is ready to be transferred. The Secondary Device will confirm that the channel is open for data. When the MCP215x or MCP2140 confirm that the channel is open for data, they will also drive the appropriate signal (CD or DSR) low to indicate that the link is now open, and Data may be transferred.
PTM Veröffentlicht am: