Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 26
For the MCP2140, there is no Receive Data Time Window. CTS is low when the Host UART Receive Buffer has space available. When CTS falls, the entire 29 Bytes of the Host UART Receive Buffer are available. CTS will be driven high when 23 bytes are in the Host UART Receive Buffer. Again this is to “give notice” to Host Controllers that use a transmit FIFO on the UART.
PTM Veröffentlicht am: