Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 19
NRM is the state where Data and Status information is transferred back and forth. Status information is also the mechanism to verify if a link is still connected (not blocked). If the link is blocked for longer than the Link timeout, then the devices will reset to the NDM state. Whenever communication is completed, the Primary Device may shut down the link. The Secondary Device will confirm this command and both devices will return to the NDM state.
PTM Veröffentlicht am: