Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 25
The MCP215x can receive an additional 4 bytes. When 64 bytes are received, the Data will be processed, formatted, and then transmitted to the Primary Device. If the Host UART Baud rate is 19200, then the Receive Data Time window will close, which forces CTS High, before 64 Bytes could be received. The Data in the Host UART Receive Buffer will be processed, formatted, and then transmitted to the Primary Device. Any data that is being received when CTS is driven high will not be lost.
PTM Veröffentlicht am: