Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 12
There are three states that the IrDA Standard protocol stack could be in. Normal Disconnect Mode (NDM), Discovery Mode, and Normal Response Mode (NRM). NDM is the state where the Primary Device is searching for other IrDA Standard devices (with the same Application Layer Protocol) and the Secondary Device is waiting for interrogation from a Primary Device.
PTM Veröffentlicht am: