Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 14
Here the Primary Device sends out XID commands. The XID command will indicate a timeslot, typically 0 to 7 depending on the IrDA Standard Stack used. When the Secondary Device gets in range of the Primary Device, it will respond to one of these XID commands, claiming that timeslot. This Secondary Device will then ignore the remaining XID commands.
PTM Veröffentlicht am: