Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 23
This Window is 22ms and the MCP215x Host UART Receive Buffer is 64 Bytes. So the Host Controller can transfer data for this 22ms up to a maximum of 64 Bytes. The table shows how many bytes can be transferred in 22ms at a given baud rate. Baud rates 19200 Baud and below will not be able to transfer the 64 Bytes in the Window time. With a Baud rate 57600 and Greater, the 64 Byte limit can be reached.
PTM Veröffentlicht am: