Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 21
Occasionally the Host Controller may be busy and not able to receive things from the Protocol Handler. For this, the Host Controller can control the state of the RTS signal. This indicates when the Protocol Handler can transmit the data it has received from the Primary Device on to the Host Controller. If the RTS signal is de asserted too long, while the Protocol Handler has data pending for the Host Controller, the link will be closed.
PTM Veröffentlicht am: