Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 17
Now it is time for the capabilities of each device to be determined. These capabilities include: IR Baud Rate, Data Packet Size, Turn Around times, and a few other things. So the Primary Device will send its capabilities, and the Secondary Device will respond with its capabilities. The Highest common denominator will then be used to optimize system performance. Now it is the responsibility of the Primary Device to send the Open Channel for Data.
PTM Veröffentlicht am: