Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
MSP430L092 Introduction Slide 9

The Analog Pool can be configured as an 8-bit DAC, ADC, SVM and Comparator. TI has named this peripheral a “pool” because it is simply that. It is a pool of analog resources that an application can pull from to accomplish a particular analog function, whether it be a comparator, DAC or A to D converter. The ADC can also be used more specifically for something like an SVM or a supply voltage monitor or temperature sensor, which will be shown in a later slide. The two main resources or building blocks are the comparator and this low voltage reference. The low voltage reference, which will be used in large part to create TI’s DAC or their digital to analog converter, is the simpler of two.

PTM Veröffentlicht am: