Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
MSP430L092 Introduction Slide 37

In summary, the MSP430L092 is a general purpose, low-cost MCU that is targeted toward low-cost single-cell applications that range from consumer electronics, such as personal hygiene care, low power gadgets, or household electronics, tools or toys or games that may require some advance digital or analog functions. These native 0.9 V devices enable the entire device, including the CPU, memory, logic, as well as all digital and analog peripherals to operate at the specified Vcc. This means no voltage level translation, no charge pump or buck converter is required to maintain the operation of the device. Additionally, the 0.9 V is the voltage of a single-cell battery at the end of its lifetime which enables the application to completely exhaust the energy that a single-cell has to offer. Finally, TI provides a number of tools to enable customers to not only develop these low 0.9 V Native solutions, but also to take these solutions to production.

PTM Veröffentlicht am: