Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
MSP430L092 Introduction Slide 28

One of the benefits of staying with the L092 platform in production is that the platform, both hardware and software, are consistent from the early development stage to production. However, in the case where high volumes are needed, the economics of having two devices, an MCU and EEPROM, make the ROM C09x device much more attractive. When discussing the ROM version, this presentation will point out the emulation mode that swaps the L device memory. This enables the same code used in the L development hardware to be used in the C production hardware.

PTM Veröffentlicht am: