Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
MSP430L092 Introduction Slide 26

There are two options to order the MSP430 development tools. The first option is to order the L092 Target Board, as well as the Active Cable. It is a complete development tool assuming that an MSP430 USB-FET is available. Alternatively, the MSP430 USB-FET can also be combined with the kit as the second option for the ordering. Not only as an evaluation platform, these development kits can also be used for application prototyping, as well as reference designs for users own application development. Once their L092 application reaches the final step of its development cycle, it will then become important to determine a production plan.

PTM Veröffentlicht am: