Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
MSP430L092 Introduction Slide 33

Choosing to produce with the C09x will require an additional development step: this is emulating the C092 with the L092. This is a quality measure to ensure that there are absolutely no issues or unexpected behavior as the memory map changes. The key to moving from the RAM-based L092 to the ROM-based C09x is the emulation mode. The emulation mode changes or swaps the memory addressing so that the L092, from the perspective of the addressing, looks like the C092. The benefits of the emulation are two-fold. First, the emulation compiles and generates the production ROM mask. The second benefit is the ability to test and validate the production mask instead of code that is one-step removed from the final production mask.

PTM Veröffentlicht am: