Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
MSP430L092 Introduction Slide 34

As this presentation has mentioned previously, the memory swap remaps the memory so that the application code in RAM looks like the ROM space within the C092. This table helps visualize and highlight the changing in the addressing. The swap is between the address of the loader code, which is physically ROM, and the application code, which is physically RAM.

PTM Veröffentlicht am: