Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
MSP430L092 Introduction Slide 21

The Target Board consists of a TSSOP 14-pin socket for easy device interchanging. It also provides breakout pins for external connectivity or to add on a prototyping board. It also contains an on-board EEPROM, which operates at 3 V; therefore, there is external circuitry required between the L092 and EEPROM to enable this cross voltage communication. The L092 Target Board also has a mini-JTAG connector to connect to the Active Cable Board. On the right-hand side of the screen is a picture of the board.

PTM Veröffentlicht am: