Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
MSP430L092 Introduction Slide 32

The L092 loader code, located in ROM, represents the third and final tool that TI provides to enable production with the L version. In addition to the loader application, an API allows the user application to access these functions and services that are located within ROM. There are sixteen API functions in addition to the loader entry function that are described in the loader code user’s guide. The public functions and services of the loader code, in addition to the reference designs for both the adaptive network and the boost circuit, help move from development with the L version to production of the L version. This presentation will now look at what are the tools that allow development with the L and then transitioning to production with the C.

PTM Veröffentlicht am: