Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Topic 4 Control Subsystem Slide 11

For the control side ROM, the size is 64 kBytes. On top of the boot loader code, C28x ROM contains some mathematic tables such as the PLC math tables, and these are additional over what is currently in octave. There is also an IQ math table, FPU math tables and some IPC handline code. However, the C28x ROM does not include a flash API, so the API will not be ROM’d, only the C28x core can access its ROM block, it can not be accessed from the DMA or the M3 side.

PTM Veröffentlicht am: